ECAT.ENRXWARN

Description

ECAT.ENRXWARN allows enabling/disabling warning W7011, which is triggered when Rx data is received from the EtherCAT master before the drive finished preparing its TX data within a sync0 cycle.


  • This warning will not be triggered when running at 250 μs cycle times as it is normal for the TX data to be from the prior cycle at this rate..
Value Description
0 W7011 cannot be triggered
1 W7011 can be triggered

Versions

Action Version Notes
Implemented 02-06-03-000 -

General Information

Type

NV Parameter

Units

N/A

Range

0 to 1

Default Value

1

Data Type

Integer

Variants Supported

Fieldbus variants: AKD2G-SPE

Industrial Ethernet Information

(missing or bad snippet)